Merkene våre

Impact-Company-Logo-English Black-01-177x54

Velkommen til nettstedet til Schneider Electric

Velkommen til nettstedet vårt.
		
Hvordan kan vi hjelpe deg i dag?
What is the China RoHS symbol - 50 inside a circle with two arrows?

This China RoHS symbol refers to the fact that the particular meter will not release hazardous substances into the environment until 50 years after its manufacturing date. Detailed information can be found at the official web page:
http://www.chinarohs.com/index.html

China RoHS