Merkene våre

Impact-Company-Logo-English Black-01-177x54

Velkommen til nettstedet til Schneider Electric

Velkommen til nettstedet vårt.
		
Hvordan kan vi hjelpe deg i dag?
What is the difference of H class and F class in Tricast cast resin dry type transformers ?
The main difference is that the class designations refer to the withstand temperature of the insulation material in Tricast cast resin dry type transformers. Thus, H class has a wihstand temperature level of 180 ⁰C for the coils and F class of 155 ⁰C for ambient design temperature of 40 ⁰C.