Merkene våre

Impact-Company-Logo-English Black-01-177x54

Velkommen til nettstedet til Schneider Electric

Velkommen til nettstedet vårt.
		
Hvordan kan vi hjelpe deg i dag?
Does Vijeo Designer Support the Allen Bradley Micro800 series PLCs?

Article available in these languages: Spansk, Japansk

Issue:
Unable to find documentation regarding support for the Allen Bradley Micro800 series in Vijeo Designer.

Product Line:
Vijeo Designer (all versions)

Resolution:
Vijeo Designer currently does not support the Allen Bradley Micro800 series of PLCs natively. In order to program a Magelis HMI to talk to the Allen Bradley Micro800 series of PLC, we must use the Modbus TCP/IP protocol. In other words, the Modbus Communication module must be installed on the Allen Bradley Micro800 PLC and the Vijeo Designer application must use the Modbus TCP/IP driver.