Merkene våre

Impact-Company-Logo-English Black-01-177x54

Velkommen til nettstedet til Schneider Electric

Velkommen til nettstedet vårt.
		
Hvordan kan vi hjelpe deg i dag?
Video: How to download Advantys island configuration (STB NIP <example>) through TCP/IP ?

Follow these steps to download Advantys island configuration (STB NIP <example>) through TCP/IP :


1. Open the Advantys configuration software and browse the configuration backup and open it
2. RIght click on island name and build the configuration
3. Go to online > Connection settings
4. Select the connection type as TCP/IP and enter the IP address of the Advantys STB NIP <example> module
5. Go to online > Click connect > Click on download option to start the download