Merkene våre

Impact-Company-Logo-English Black-01-177x54

Velkommen til nettstedet til Schneider Electric

Velkommen til nettstedet vårt.
		
Hvordan kan vi hjelpe deg i dag?
On the ATV320 can motor rotation be reversed using programming?
Issue:
ATV320 reverse motor rotation with programming.

Product Line:
Altivar 320

Environment:
All

Cause:
Need to reverse motor rotation

Resolution:
No, the ATV320 does not have this functionality in the programming. Two motor leads will need to be swapped in order to reverse motor rotation.