Issue:
Needs to connect a 4-20ma speed reference to a ATV340 drive
Product Line:
ATV340
Environment:
All
Cause:
Needs 4-20ma analog input
Resolution:
The 4-20ma speed reference must be connected to AI1 and COM. Using the VW3A1111 keypad, this has to be setup in the drive as follows:
in Complete settings, go to Input/output menu.
Press the button under the AI/AQ tab at the bottom of the screen
Go to AI1 configuration and set AI1 type to current.
Then change AI1 min value to 4.0ma.
Factory default has Ref freq 1 config set for AI1 so that will not need to be changed. Now the drive is setup for 4-20ma speed reference.
Publisert for: Schneider Electric Norway