How can we help you today?

How to perform a warm or cold logic restart in SCADAPack x70 device using logic

Use the Device_ExecuteCommand function block in ScadaPack logic engine to execute a subset of the SCADAPack command-line functions. The command is passed to the function block as a string and is executed by the SCADAPack when triggered.

Use 'RESTART LOGIC WARM' or 'RESTART LOGIC COLD' as an input string passing to CMD pin of the block to perform a warm logic restart or cold logic restart.

Logic engine

Help doc

Schneider Electric New Zealand

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product:
  • Products Documentation
  • Software and Firmware
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre
  • Where to Buy?
  • Office Locations
  • Schneider Electric, PDL & APC Phone: 0800 741 303
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
  • Conditions of Sale
  • Change your cookie settings
  • Preference Centre