The Micrologic Communications Adapter (CIM3F) links Micrologic circuit breaker trip units to a Powerlogic system. The communications cable connector is used to connect the communications adapter to the Powerlogic Product Interface (Class 3050 Type PIF-3) for Micrologic circuit breakers. The product interface works with the communications adapter to make circuit breaker trip unit information accessible to the Powerlogic system. The CIM3F is compatible with LE, ME, NE, PE, and SE Frame Circuit Breakers.
Legacy KB System (APS) Data: RESL198100 V1.0, Originally authored by AnVa on 03/21/2009, Last Edited by AnVa on 03/21/2009
Related ranges: Communication with Micrologic trip units, Series III MicroLogic Trip Unit Interface (PIF3)
Publicado para: Schneider Electric Portugal