Pesquisar nas perguntas frequentes (FAQ)
What is the degree of protection for the open style ATS22 softstart?
Issue:
Degree of protection for the open style ATS22 softstart
Product Line:
ATS22, Altistart 22
Environment:
All models
Cause:
N/A
Resolution:
The Altistart 22 soft starter is considered an open type device. A conduit kit is not available to convert these to NEMA 1. The IP rating is IP20.
If higher protection is needed a custom enclosure or a standard enclosed ATS22 softstart may be required
Publicado para:Schneider Electric Portugal
Explorar mais
Gama:
Explorar mais
Gama: