Pesquisar nas perguntas frequentes (FAQ)
Does Somachine support ZBRN1 DTM?
Issue:
Looking for confirmation of support for ZBRN1 DTM in SoMachine
Product Line:
SoMachine
Resolution:
SoMachine v3.1 did not support the ZBRN1 DTMs. It supported only ZBRN2 which are for serial communications. The Harmony DTM is supported in SoMachine V4/V4.1 and onwards versions but not in V3.1.
The DTM can also be added to SoMachine V3.1 but it is validated for SoMachine versions > V4
(See Release notes of SoMachine)
Note: Only DTM for serial communication (ZBRN2) can be used in SoMachine V4.1 - Modbus TCP is not possible that time with SoMachine v4.1 (ZBRN1)!
Today if we check with SoMachine version v4.3, we can add ZBRN1 as Modbus TCP/IP slave
Note: Only DTM for serial communication (ZBRN2) can be used in SoMachine V4.1 - Modbus TCP is not possible that time with SoMachine v4.1 (ZBRN1)!
Today if we check with SoMachine version v4.3, we can add ZBRN1 as Modbus TCP/IP Server