Issue:
How can you connect Somove using the CANopen connection option?
Product Line:
ATV61, ATV71, ATV320 and ATV340 only
Environment:
All
Cause:
Connection using CANopen
Resolution:
You will need to use a CANopen USB-CAN Dongle ( Port 1 only is supported) if you have a dual port.
This connection option is only supported with the ATV61, ATV71, ATV320 and ATV340 Drives only. You can not use this option on the ATV630 or ATV930 drives.
See the attached document on setting up Somove to use CANopen.
Publicado para: Schneider Electric Portugal