Search FAQs
Osisense XC - Contact diagram of the limit switch ZCMD21L* or ZCMD21C12 + ZCE13 steel ball bearing plunger
Please find hereafter the contact diagram of the limit switch ZCMD21L* or ZCMD21C12 (5-pin M12) + ZCE13 steel ball bearing plunger. It is not shown into the Limit switches XC standard catalogue. ZCMD21M12 (4-pin M12) + ZCE13 has the same diagram too
Released for:Schneider Electric Saudi Arabia
Attachment(s)
Explore more