Våra varumärken

Välkommen till Schneider Electrics webbplats

Välkommen till vår webbplats.
		
Hur kan vi hjälpa dig idag?
On the Class 8536 starters, what is form B5?
Issue:
"B5" modification for used on NEMA Starters

Product Line:
8536 8538 8539 Type S Full Voltage Contactors and Starters

Product Line:
NEMA Starters, Type S, Pre Type S

Resolution:
This Form was obsoleted in 2002.
Form B5 was for Non-compensated, bimetal overload relay.

Substitute non-compensated bimetallic overload relays on Type S or a separately mounted IEC style overload.  (i.e. LRD or LR9F series).