The Altivar 312 and Altivar 71 cannot be connected on the same DC bus.
The Over Braking Fault (OBF ) threshold of ATV312 is 880V and the OBF of ATV71 is 825V .That make incompatible both the products connected in same DC bus.
Publicerad för:Schneider Electric Sverige