What is maximum number of cycles per hour for Altistart 01.
Please refer the attached below table with the maximum number of cycles per hour according to the starting time and the rated operating current.
| Ie = rated operating current | |||
| 5 x Ie | 6 x Ie | ||
| Starting time | Maximum number of cycles per hour | ||
| 1 | 100 | 60 | ATS01N1 |
| 5 | 20 | 12 | |
| 1 | 100 | 60 | ATS01N206…222 |
| 5 | 20 | 12 | |
| 10 | 10 | 6 | |
| 1 | 50 | 30 | ATS01N232 |
| 5 | 10 | 6 | |
| 10 | 5 | 3 | |