How to calculate the efficiency value of Altivar 12.
Efficiency is the ratio of (Drive power) and  (Drive power + losses)
The losses are giving in Altivar 12 catalog ( Refer the attached file )

Example for ATV12HU22M2
Power=2.2 Kw
Losses=93W
Efficiency (at 100% of load) = (2200)/ (2200+93) =95.94%

Schneider Electric Sverige

Bilagor
ATV12_Losses.pdf [121.99 KB]
Utforska mer
Produktfamilj
Artiklar som kan vara till nytta
Utforska mer
Produktfamilj