Våra varumärken

Välkommen till Schneider Electrics webbplats

Välkommen till vår webbplats.
		
Hur kan vi hjälpa dig idag?
How to use PRESET H-METER(Preset Hour Counter)Function Block in Zelio Logic.
PRESET H-METER (Preset Hour Counter)Function Block(FB) will active a output of FB when the first input of FB is at TRUE during
a delay determine by configuration. The accuracy of PRESET H-METER Function Block in FBD (Function Block Diagram)
is 1second + 2 Time cycle. Refer to attached sample program using PRESET H-METER Function Block in FBD Mode.

Schneider Electric Sverige

Bilagor
PRESET H-METER _Zelio.zip [3.33 KB]