Våra varumärken

Välkommen till Schneider Electrics webbplats

Välkommen till vår webbplats.
		
Hur kan vi hjälpa dig idag?
How to order Harmony XKB Joystick Controller with analogue output.

To order a Harmony XKB Joystick Controller with analog output, the user must use a Zelio Analog Interface module, such as the RMCN22BD or RMCL55BD, configured for a 4–20 mA analog output.
These modules function as current generators in conjunction with the joystick’s potentiometer. The potentiometer itself operates within a 0–10 V signal range, which is then converted to the desired current output.