All Modicon M258 controllers have two groups of high-speed Inputs/Outputs with, for each group:
Four sink type high-speed inputs(up to 200 KHz),2 standard inputs and 2 source type high-speed outputs (up to 100 KHz) dedicated
to HSC( High Speed Counter) or PWM (Pulse Width Modulation) functions.
to HSC( High Speed Counter) or PWM (Pulse Width Modulation) functions.
A high-speed input which can be used as an “Encoder capture input”
Two commons for the inputs.
One common for the outputs.
A power supply (24VDC) consisting of 3 units:
One for the CPU (Control Processing Unit).
One for the high-speed Input/Output modules.
One for other modules (Internal Input/Output Bus).
Publicerad för:Schneider Electric Sverige