Is it possible to use two Extended I/O Cards in one Altivar 71 drive.
It is not possible to use two I/O Extension cards in one Altivar 71 drive. However, it is possible to use one VW3A3201 Logic I/O
Card & one VW3A3202 Extended I/O Card in one Altivar 71 drive. Refer to attached file for Option Card compatibility.

Schneider Electric Sverige

Bilagor
Option Card compatibility table_ATV71.pdf [21.35 KB]
Utforska mer
Produktfamilj
Artiklar som kan vara till nytta
Utforska mer
Produktfamilj