Can the ATV312 be used to control speed of the motor with 0-10 mA?
Issue:
mA signal configuration on the ATV312 Drive

Product line:
Altivar ATV312

Environment:
All models, all serial numbers

Cause:
This drive uses terminals AI3 and COM for the mA signal.  It can be configured as 0-20mA or 4-20mA.

Resolution:
Under the I-O_ menu go to CRL3 to adjust the minimum value and CRLH to adjust the maximum value.

Schneider Electric Sverige

Utforska mer
Produktfamilj
Artiklar som kan vara till nytta
Utforska mer
Produktfamilj