Våra varumärken

Välkommen till Schneider Electrics webbplats

Välkommen till vår webbplats.
		
Hur kan vi hjälpa dig idag?
How do I compare drive configuration files with SoMove?
Issue:
SoMove files configuration comparison.

Product Line:
ATV312, ATV32, ATV320, ATV61, ATV71, ATV600, ATV900, ATS48, ATS480,ATS22

Cause:
None

Resolution:
In order to compare configurations between two drives using SoMove, both drives have to be the same model numbers and both configuration files should be saved.
1. Open one of the configurations
2. Select "Compare Configurations" from the File menu
3. Select the configuration file of the device that you want to compare
Both configuration files will be displayed on the screen.  The values highlighted are those parameters that are different.