Våra varumärken

Välkommen till Schneider Electrics webbplats

Välkommen till vår webbplats.
		
Hur kan vi hjälpa dig idag?
It's possible to Know the percent of tollerance of input (AIC) 0-20 / 4-20 mA (+/- = ?)

Goals and Symptoms

It's possible to Know the percent of tollerance of input (AIC) 0-20 / 4-20 mA (+/- = ?)

Facts and Changes

Percent tollerance ATV18(AIc)

Causes and Fixes

The accuracy +/- 5%.


Legacy KB System (APS) Data: RESL157496 V1.0, Originally authored by on , Last Edited by on
Related ranges: Altivar 18