Issue
What is the ProWORX NxT Logbook used for?
Product line
ProWORX
Environment
ProWORX NxT
Resolution
The Logbook is a general purpose note holder that is attached to a database name but is not linked to any database record. It can be used as a scratch pad to remember information, as a daily journal, or a reminder pad to pass information between different shifts. You can automatically display the Logbook on entry into the network editor. This forces the next user (for example, the following shift) to review the logbook.
Publicerad för: Schneider Electric Sverige