Våra varumärken

Välkommen till Schneider Electrics webbplats

Välkommen till vår webbplats.
		
Hur kan vi hjälpa dig idag?
Can I convert an XBTL1000 application (XBTF terminal) to Vijeo Designer (XBTGT/GK terminal)?

We have a Services & Projects offer making it easy to migrate XBTL 1000 applications created on XBTF terminals to Vijeo Designer applications for use on XBTGT/GK HMI terminals.

The service provides:

  • Analysis of the complexity of migration regarding hardware, software, communication with PLCs, etc.
  • Analysis of the new functional requirements
  • Proposal for migration methodology
The possible deliverables include:
  • Simple conversion
  • Full migration of complex machines
  • Migration to SCADA system
  • Standardisation process for multiple machines

The Software to migrate from XBTL1000 to Vijeo Designer v5.1 is called "Switch2Vijeo". Please contact the Customer Care Center for further information about the migration service.

Note: Migration cannot be performed by the end user.

Note: The software XBTL1000 the XBTF terminals and the XBTGT/GK ranges are now obsolete The Magelis HMI GTO is the nearest current range.