Våra varumärken

Välkommen till Schneider Electrics webbplats

Välkommen till vår webbplats.
		
Hur kan vi hjälpa dig idag?
What product line replaces the Class 8839 PowerGard CPA CPC CPD 18-pulse drives?
Issue:
Need a replacement for the Class 8839 PowerGard CPA CPC CPD 18-pulse drives?

Product Line:
PowerGard Class 8839

Environment:
All

Cause:
Replacement or new application

Resolution:
The PowerGard 18-pulse drive product line is obsolete.  The ATV680 and ATV980 product lines are the functional replacements. These are Active Front End units.