Våra varumärken

Välkommen till Schneider Electrics webbplats

Välkommen till vår webbplats.
		
Hur kan vi hjälpa dig idag?
What are the replacement CT's or current transformers for the ATS48C66Y soft starter?
Issue:
What are the replacement CT's or current transformers for the ATS48C66Y soft starter?
Product Line:
Altistart ATS48
Environment:
All
Cause:
Replacement parts needed.
Resolution:
CT's are part of the bus bar assembly VZ3N005S48 however this part is not available to purchase. One option is to return the Soft Start for repair.