Våra varumärken

Välkommen till Schneider Electrics webbplats

Välkommen till vår webbplats.
		
Hur kan vi hjälpa dig idag?
What can cause an CRF fault on the ATV31 and ATV312 drives?
Issue:
CRF fault on the ATV31/ATV312 drives.

Product Line:
Altivar ATV31 and ATV312

Environment:
All

Cause:
Powered down the drive and when they powered it back up it tripped on CRF and will not clear.

Resolution:
CRF is an internal precharge fault.  Power cycle.  If the fault does not clear you will need to replace the drive.

Schneider Electric Sverige

Bilagor
Program BBV46385_03 ATV312.pdf [2.6 MB]