Våra varumärken

Välkommen till Schneider Electrics webbplats

Välkommen till vår webbplats.
		
Hur kan vi hjälpa dig idag?
What are the screen resolutions that are supported under Generic PC Runtime in Vijeo Designer v6.2?
Issue:
What are the screen resolutions that are supported under Vijeo Designer Generic Windows PC Runtime?

Product Line:
Screen resolution, 4:3, 16:9, aspect ratio, 1080p, 1080i, 720p

Environment:
Generic Windows PC Runtime, Vijeo Designer

Resolution:
Below are the list of display resolutions available for the generic PC runtime:
800 x 600 (SVGA)
1024 x 768 (XGA)
1280 x 720 (HD720)
1280 x 1028 (WXGA)
1366 x 768 (FWXGA)
1440 x 900 (WSXGA)
1600 x 1200 (UXGA)
1680 x 1050 (WSXGA+)
1920 x 1080 (HD1080)
1920 x 1200 (WUXGA)
2560 x 1600 (WQXGA)

Keep in mind that the limitation of the resolution usually depends on the graphics chip on the industrial PC and monitor that are used.