Våra varumärken

Välkommen till Schneider Electrics webbplats

Välkommen till vår webbplats.
		
Hur kan vi hjälpa dig idag?
Does the ATS01 softstart require external thermal overload protection?
Issue:
Is an external thermal overload protection needed to be installed with an ATS01?

Product Line:
ATS01, Altistart 01

Environment:
All

Cause:
N/A

Resolution:
The ATS01 softstart does not provide motor overload protection.  Separate overload thermal protection should be added to the power circuit.  This typically is done with a motor starter upstream of the ATS01.