Våra varumärken

Välkommen till Schneider Electrics webbplats

Välkommen till vår webbplats.
		
Hur kan vi hjälpa dig idag?
Cannot assign located variable to the Unity Momentum IO
Issue
Cannot assign located variable to the Unity Momentum IO

Product Line
Unity Momentum 171CBU*****

Environment
Unity, Control Expert

Resolution
Located variables cannot be assigned to the Momentum IO as in Concept.

Typically, the hardware configuration information is stored in %KW words for the Unity PLC's.  Due to the hardware
limitation, the use of %KW words is not allowed for the Momentum PLC.  As a result, Unity is forced to use reserved
%MW words for the module configuration information.  The %MW words used for the configuration are intentionally
locked out to prevent the user from changing the values.  This also locks out the the use of a %MW assignment for the IO.