What is recommended TORQUE for screws on SCADAPack 32 and SCADAPAck 300 I/O terminals?For I/O removable terminal blocks (6,8,9 and 10 pole, 12 to 22 AWG and 15A contacts screw termination), recommended is 6 lb.-in. (0.68 Nm) torque.
Publicerad för:Schneider Electric Sverige