Sök bland vanliga frågor (FAQ)
Osisense XC - What is the material of the spring rod head ZCKD08?
The spring rod head ZCKD08 uses a spring made of stainless steel closed to the SUS 302 or AISI 302, without any surface threatment. The ZCKD08 head is associated to the ZCKM or ZCKS (black color) contact body. The spring rod head ZCKE08 uses a spring with such material too. The ZCKE08 head is associated to the ZCKJ contact body
Publicerad för:Schneider Electric Sverige
Bilagor
Utforska mer
Utforska mer