Våra varumärken

Välkommen till Schneider Electrics webbplats

Välkommen till vår webbplats.
		
Hur kan vi hjälpa dig idag?
Is it possible to set the date and time on all Sepam series 10 versions?
Only Sepam 10A has the option of time and date stamping as it is the only version that can have time-tagged event recording that is why it is the only version where it is possible to set the date and time. Sepam 10 version B and N do not have this time-tagged recording option thus they do not have a real-time clock.

AEDL3