Våra varumärken

Välkommen till Schneider Electrics webbplats

Välkommen till vår webbplats.
		
Hur kan vi hjälpa dig idag?
Is the OFS server designed only to run under the active users when it is running as process only.
Issue
Is the OFS server designed only to run under the active users when it is running as process only.

Product Line
OPC Factory Sercer (OFS)

Environment
Windows 10 version 1902, OFS v3.62

Resolution
OFS is configured through DCOM to run with the Interactive user identity, that is the logged user.