Våra varumärken

Välkommen till Schneider Electrics webbplats

Välkommen till vår webbplats.
		
Hur kan vi hjälpa dig idag?
Is the registration of TwidoSuite software compulsory?
The registration of TwidoSuite is compulsory.

TwidoSuite is sold as a DVD-ROM, part number TWDBTFU10M, or downloaded free of charge.

Please note the software must be registered before the 30-day trial period expires. If it is not registered within this period, it must be uninstalled and re-installed and then registered.


Important information:
The Twido range is discontinued and the possible replacement is the Modicon M221. The software to program this new controller is the EcoStruxure Machine Expert Basic also free.
The software can automatically be migrated to this new platform but check with our support center your architecture to validate the migration.

Link:

EcoStruxure Machine Expert Basic V1.3 | Schneider Electric