How can you remotely connect the VW3A1111 (Remote keypad) to the Altivar Process drive?

Article available in these languages: Japanska

Issue:
Connect the Remote Keypad (VW3A1111) to the Altivar Process drive

Product line:
ATV600, ATV900, Altivar Process

Environment:
All Altivar 600 and 900 process drives

Cause:
N/A

Resolution:
The VW3A1111 keypad has a cable port built into the bottom.  Move the rubber cover to access the port.  See the photo attached.
This is generally a temporary connection.  To permanently remote mount the keypad, use VW3A1112.

Schneider Electric Sverige

Bilagor
keypad edge photo.JPG.jpg [257.32 KB]
Utforska mer
Produktfamilj
Artiklar som kan vara till nytta
Utforska mer
Produktfamilj