Våra varumärken

Välkommen till Schneider Electrics webbplats

Välkommen till vår webbplats.
		
Hur kan vi hjälpa dig idag?
Unity Pro : Use of operation on index in INC or DEC function causes a Build error
Goals and Symptoms

When building an application using operation on index in INC or DEC function the build fails with following error message : error during the ARM assembler phase
Code generation failure

Example:  INC(my_array[ind*3+1]);

The problem is in Unity Pro V8.0 to V11.0.

Causes and Fixes:
The workaround consits to program the operation outside the function.

Example :
Ind1 :=ind*3+1 ;INC(my_array[ind1]);