Våra varumärken

Välkommen till Schneider Electrics webbplats

Välkommen till vår webbplats.
		
Hur kan vi hjälpa dig idag?
Where are the auto start terminals for auto mode on the enclosed ATV660 Process drives?
Issue:
Looking for the auto start terminals for auto mode on the enclosed ATV660 Process drives

Product Line:
Enclosed only ATV660

Environment:
Altivar ATV660 enclosed drives.

Cause:
Where is the auto start to start the drive in auto mode?

Resolution:
TB-1  contacts 3 and 4 are the auto start terminals for auto start.