Våra varumärken

Välkommen till Schneider Electrics webbplats

Välkommen till vår webbplats.
		
Hur kan vi hjälpa dig idag?
Controlling a point in ClearSCADA Mobile
This article describes the steps to take in order to control a point (analog or digital) in the ClearSCADA database using ClearSCADA mobile.

Follow these steps to control a point from ClearSCADA mobile:

1) In the ClearSCADA configurator go to Global Settings.  Right-click and select 'Update Settings'.  Set the 'Controls Allowed' field to 'Yes'






2) As per the ClearSCADA mobile help manual (search 'control' in the ClearSCADA Mobile - Administration Guide), add the MobileControlsAllowed metadata field and label










3) On the 'Identification' tab of the point (analog or digital), check the 'Mobile Controls Allowed' checkbox.






4) Create a 'Mobile Display' object in ViewX







5) On the mobile device, go to the 'Displays' area to control each point














6) Verify the changes on the mimic in ViewX or WebX