Våra varumärken

Välkommen till Schneider Electrics webbplats

Välkommen till vår webbplats.
		
Hur kan vi hjälpa dig idag?
What is the speed accuracy in percentage of the ATV930 drive when used with a closed loop encoder or when used in Sensorless Vector Control (SVC) in open loop?
Issue:
ATV930 drive:
  • Percent of speed accuracy achievable with a closed loop encoder
  • Speed regulation when used in open loop mode

Product Line:
ATV930 drives

Environment:
Closed Loop encoder

Cause:
Speed Accuracy / Speed Regulation

Resolution:
For ATV930 drive,
The AC Drive shall provide a speed accuracy 0.01 % of the nominal speed of the motor, in closed-loop mode, with an encoder.
The drive has a speed accuracy within 5% of the nominal motor slip when operating in open loop sensorless vector mode.