Våra varumärken

Välkommen till Schneider Electrics webbplats

Välkommen till vår webbplats.
		
Hur kan vi hjälpa dig idag?
How can I ensure the class 2 during installation of my Resi9 Electrical Panel ?

If the Electrical Panel is set directly on the wall, there is a need to add an insulated backpart to your base Electrical Panel.
If installed on trunking system or recessed tray there is no need to add additional accessories.

For more details please click : https://www.se.com/ww/fr/FR/download/document/NVE1357501