Våra varumärken

Välkommen till Schneider Electrics webbplats

Välkommen till vår webbplats.
		
Hur kan vi hjälpa dig idag?
How to program an ATV630 (Process) drive to use the keypad for start/stop and AI1 for 4-20mA speed reference.

Issue:
ATV630 (Process) drive set up with keypad as start/stop and AI1 as 4-20mA speed reference.

Product Line:
Altivar ATV630

Environment:
All

Cause:
Programming

Resolution:
From main menu, go into to menu 5 (complete settings).
Scroll down to menu 5.5 menu (Command and reference) and press OK.
Set Ref Freq 1 config to AI1.
Set control mode to separate.
Set Cmd channel 1 to HMI.
ESC back to Complete settings menu.
Scroll down to menu 5.11 Inputs/Outputs menu.
Select AI/AQ tab.
Enter on AI1 configuration.
Set analog input type to current.
Set AI1 min value to 4mA.
Set AI1 max value to 20mA.

If this FAQ did not solve your issue, you can call us at 1-888-778-2733 Option 2 and then 4 or e-mail us at drive.products.support@se.com to create a case with our Technical Support Team.