What do "angle compen", "ratio compen" mean for IEM3455?
If the  LVCT selected have the angle and ratio compensation values specified on it, the same needs to be configured into the meter with which it is used.

This clarification will be added in an upcoming release of iEM3000 user manual.

Schneider Electric Sverige