Våra varumärken

Välkommen till Schneider Electrics webbplats

Välkommen till vår webbplats.
		
Hur kan vi hjälpa dig idag?
What is the Short Circuit (AIC) rating for Circuit Breakers inside the ATV660 Drive System?
Issue:
Short Circuit (AIC) rating for Circuit Breakers inside the ATV660 Drive System.

Product Line:
ATV660, Process Drive System

Environment:
All

Cause:
NA

Resolution:
All Altivar 660 Process Drives include a circuit breaker as a disconnect device and
have a short-circuit rating of 100,000 A at up to 480 V.