Internal: How do I connect a GV2P/GV3P circuit breaker to an ATV320B drive?

**Internal**
Issue:

Connecting a GV2P/GV3P circuit breaker to an ATV320B drive.

Product Line:
ATV320xxxxxB variable frequency drives

Environment:
All ATV320 part numbers ending with "B"

Cause:
Information difficult to find.

Resolution:
Two parts are needed.  One to make the mechanical connection and one to make the electrical connection. The part is the same for all ATV320xxxxxB drives regardless of input voltage or horsepower.   The part numbers are as follows:

Part# VW3A9921 - Bracket for direct mounting of the GV2 to the ATV320B drive
Part# GV2AF4 - Electrical adapter plate for connecting the GV2 to the input of the ATV320B.


Schneider Electric Sverige

Utforska mer
Produktfamilj
Artiklar som kan vara till nytta
Utforska mer
Produktfamilj