Våra varumärken

Välkommen till Schneider Electrics webbplats

Välkommen till vår webbplats.
		
Hur kan vi hjälpa dig idag?
ATV212 S-flex - What is the "output power percentage" scaled from?
Issue:
On the ATV212 series drive, "Output power" is displayed as a percentage.  What is the reference for this scale?

Product Line:
ATV212 series drives

Environment:
All models, All serial numbers.

Cause:
Information unavailable in current literature.

Resolution:
The Output Power percentage, as read over the network, is a percentage of the rating of the drive itself, not the motor.