Våra varumärken

Välkommen till Schneider Electrics webbplats

Välkommen till vår webbplats.
		
Hur kan vi hjälpa dig idag?
What is the maximum number of Email modules allowed in Power Monitoring Expert VIP
Issue
User would like to know the maximum number of email modules that can be added to a VIP node.

Product
Power Monitoring Expert (PME) 8.x, 9.0

Environment
Designer

Resolution
The maximum number of email modules a user can add is 4095.
Note: Recommend maximum size of the Vip .cfg and .bak file be less than 2 MB.