How ClearSCADA Mobile licensing works?
This is an overview of ClearSCADA Mobile licensing. For more information about the ClearSCADA Mobile components visit FA314093.

ClearSCADA Mobile Application:
  • installed on iOS or Android based mobile devices
  • does not require license to be installed
  • displays Device ID which is unique to a particular mobile device
ClearSCADA Mobile Server:
  • is licensed separately from ClearSCADA
  • the license is based on the number of systems and the number of mobile devices for each system
  • only a software license available - ClearSCADA Mobile Server does not support dongle licenses
  • licensed through ClearSCADA Mobile Configurator
  • Machine ID is required to generate a license
  • Machine ID can be found in the Licensing section of the ClearSCADA Mobile Configurator


ClearSCADA Mobile Companion
  • Does not need a separate license
  • ClearSCADA License has to allow for at least 1 ODBC connection

Schneider Electric Sverige