Våra varumärken

Välkommen till Schneider Electrics webbplats

Välkommen till vår webbplats.
		
Hur kan vi hjälpa dig idag?
How to fix Invalid SSL Certificate error in Original WebX?
The following error may be displayed in Original WebX.




The most common cause of this error is when a non-secure connection is used and the ClearSCADA server is configured to deny logon and database writes over non-secure connection. The following two options can be considered to fix this error:
  • Use secure connection instead - connect using HTTPS (recommended)
  • Re-configure the ClearSCADA server to allow non-secure connections  by navigating to Server Configuration -> System Configuration -> WebX and checking the "Allow logon and database writes over non-secure HTTP" feature